{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the terminal lug data for the HCP5086-12N I Line Panelboard interior?

Issue:
What is the lug size and wire bending wire capacity for the Main lugs of a HCP5086-12N I Line Panelboard interior?

Product Line:
I Line Panelboards

Environment:
Termination Features

Resolution:
The lug will accommodate up to (4) 3/0 to 750 kcmil Al/Cu wire per phase, but due to NEC wire bending space, only up to (4) 3/0 to 500 kcmil Al/Cu wire, per phase,  may be terminated to the Main lugs.

Schneider Electric USA