Issue:
9999SP28R field install
Product Line:
NEMA Contactors and overload relays
Environment:
Cover-Mounted Control Units
Resolution:
It is the 9001KP1R31.
9999SP28R is the pilot light used for electrically held. The same pilot light assembly can't be used for mechanically held because of coil clearing contact. Customer can use half of the snap switch that is not being utilize by the lighting contactor as a power source. Suggest to use 9001KP pilot light instead and wire it up themselves from the snap switch.
9999SP28R field install
Product Line:
NEMA Contactors and overload relays
Environment:
Cover-Mounted Control Units
Resolution:
It is the 9001KP1R31.
9999SP28R is the pilot light used for electrically held. The same pilot light assembly can't be used for mechanically held because of coil clearing contact. Customer can use half of the snap switch that is not being utilize by the lighting contactor as a power source. Suggest to use 9001KP pilot light instead and wire it up themselves from the snap switch.