{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What type of fuses are required in Schneider Electric 9070 Type T or Type TF control transformers?

Issue:
Fuses needed to install in the Fuse Blocks of some 9070 Class Control Transformers


Product Line:
LV Control Transformers


Environment:
Applies to Fused Control Transformers by SquareD/Schneider Electric


Cause:
Fuse Blocks for 9070 Class Control Transformers are not supplied with fuses from the factory

Resolution:
Two Class CC fuses, time delay, rejection type are needed on the primary and one midget (11/32 x 1-1/2 inch) fuse is needed on the secondary

Schneider Electric USA