Search FAQs
Is the breaker communication module (BCM) for the Powerpact P and R frame field installable?
Issue:
Can a BCM be added to a P-frame or R-frame circuit breaker?
Product Line:
Circuit Breakers
Resolution:
Yes, a BCM can be added to a P-frame or R-frame breaker with an A, P, or H trip unit.
Note: if the P or R frame breaker includes a suffix E1, then the breaker already has a BCM included.
P-frame breaker
Unit mount - BCM catalog number S64205
I-line - BCM catalog number S64205
Motor operated - BCM catalog number S64207
Drawout - BCM catalog number S64206
R-frame breaker
Unit mount - BCM catalog number S64205
I-line - BCM catalog number S64205
Can a BCM be added to a P-frame or R-frame circuit breaker?
Product Line:
Circuit Breakers
Resolution:
Yes, a BCM can be added to a P-frame or R-frame breaker with an A, P, or H trip unit.
Note: if the P or R frame breaker includes a suffix E1, then the breaker already has a BCM included.
P-frame breaker
Unit mount - BCM catalog number S64205
I-line - BCM catalog number S64205
Motor operated - BCM catalog number S64207
Drawout - BCM catalog number S64206
R-frame breaker
Unit mount - BCM catalog number S64205
I-line - BCM catalog number S64205
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: