{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does Square D have recommendations for specification of a concrete pad for a Transformer?
Issue:
Installation of Transformers

Product Line:
Low Voltage Transformers

Environment:
Outside installation of a Low Voltage Transformer

Cause:
Transformer installation recommendations

Resolution:

It is the responsibility of the mechanical engineer on record for the project to determine the specification for the mounting pad details to the application specifics and base the specification on the weight, dimensions, and mounting detail shown in the Transformer drawing.


Schneider Electric USA