{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How many single pole QO breakers will the various Mini-Power Zone (MPZ) unit substations accommodate?
Issue:
Mini Power Zone Transformers branch breaker spaces

Product Line:
LV Transformers

Environment:
Applies to Mini Power Zone Transformers from SquareD/Schneider Electric

Cause:
Mini Power Zone Transformers have a finite number of branch breaker spaces

Resolution:
MPZ Mini-Power Zone products using the QO series breakers will accommodate:
1ph -- 5, 7.5, and 10 kVA - 10  single pole breakers; 15 and 25 kVA  - 28 single pole breakers
3ph -- 27 single pole breakers

Schneider Electric USA