Issue:
Can a PQ3610G busway be mounted in a vertical direction if the busduct is installed vertically?
Product Line:
Busway
Environment:
Installation
Resolution:
No. The PQ3610G will mount on vertical busduct, but the unit`s long dimension will be horizontal. Suggest using a PFA34100G circuit breaker unit, which will have a long dimension which follows the vertical rise of the busduct.
CTA-ID : 2010390
Can a PQ3610G busway be mounted in a vertical direction if the busduct is installed vertically?
Product Line:
Busway
Environment:
Installation
Resolution:
No. The PQ3610G will mount on vertical busduct, but the unit`s long dimension will be horizontal. Suggest using a PFA34100G circuit breaker unit, which will have a long dimension which follows the vertical rise of the busduct.
CTA-ID : 2010390
Released for:Schneider Electric USA