{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the AC and DC coils interchangeable on the LC1D115 and LC1D150 TeSys contactors?
Issue:
Changing control voltage from AC to DC or vice versa

Product Line:
IEC Contactors and Starters

Environment:
Tesys D contactors and coils

Cause:
Change from an AC to DC coil in a D line contactor

Resolution:
Yes, but only with these two contactors. They are not interchangeable on any other D-Line contactor.

Schneider Electric USA

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: