{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What does it mean when the catalog shows a XB4BVG4 (ZB4BVG4 and ZB4BV043)
Issue:
Meaning when the catalog shows a XB4BVG4 (ZB4BVG4 and ZB4BV043)

Product Line:
Push Button and Operator Interface

Environment:
22 mm Push Buttons

Resolution:
The ``X` number means complete device and the ``Z`` numbers are the components that make up the complete device.

Schneider Electric USA