{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the acceptable enclosure depth for the Powerpact P frame extended rotary handle?
Issue:
What are the acceptable lengths for the Powerpact P frame extended rotary handle?

Product Line:
Circuit Breakers

Resolution:
The distance from the back of the circuit breaker and door must be between 218 mm (8.58 in) and 605 mm (23.82 in).
See attached instructions for more detail.

Schneider Electric USA

Attachment(s)
P Rotary Handle 48049-253-01.pdf [848.87 KB]