{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
A 9002AW2 foot switch uses a 9007 AO2 industrial snap switch for 1 NC & 1 NO contact closures. Can a 9007CO3 switch be used in that foot mechanism for 2 NO & 2 NC?
Issue:
Can a 9007CO3 switch be used in that foot mechanism for 2 NO & 2 NC? A 9002AW2 foot switch uses a 9007 AO2 industrial snap switch for 1 NC & 1 NO contact closures.

Product Line:
Foot Switches

Environment:
Push Buttons and Operator Interface

Resolution:
No changes to contacts or operation of the switch can be made on any foot switch. You can replace the covers, pedal, pedal return spring, and contacts in any switch, but not modifications to contact arrangement or operation can be made.

Schneider Electric USA