{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do we offer a Tesys IEC combination starter in a stainless steel enclosure?

Issue:
Stainless steel enclosure for a Tesys D combination starter

Product Line:
IEC Enclosed Combination Starters

Environment:
IEC Contactors and Starters

Resolution:
The LE1D Tesys IEC combination starters are only available in Types 1 and 12/3R enclosures.
However, we have the Tesys N combination starters that are available in NEMA 4 and 4X stainless steel enclosures. While these are NEMA rated combination starters we use the IEC Tesys D-line.
Contactors.

Schneider Electric USA