Search FAQs
Video: What is the maximum QO or QOB branch breaker (not sub-feed breaker) that can be installed in an NQOD panelboard?
Issue:
Can QO breakers be installed in a NQOD Panelboard and what is the maximum rating?
Product Line:
Panelboard, Mini Circuit Breakers
Environment:
NQOD Panelboards
Resolution:
The maximum QO branch breaker that can be installed in an NQOD panel is a 2-pole 125Amp. The maximum QOB branch breaker that can be installed in an NQOD panel is a 2 or 3 Pole, 150Amp.
The following video demonstrates how to install 110-150A QOB VH breakers:
Can QO breakers be installed in a NQOD Panelboard and what is the maximum rating?
Product Line:
Panelboard, Mini Circuit Breakers
Environment:
NQOD Panelboards
Resolution:
The maximum QO branch breaker that can be installed in an NQOD panel is a 2-pole 125Amp. The maximum QOB branch breaker that can be installed in an NQOD panel is a 2 or 3 Pole, 150Amp.
The following video demonstrates how to install 110-150A QOB VH breakers:
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: