{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the NEMA 4X transformers listed in the Digest have aluminum or copper windings?
Issue:
Do the NEMA 4X transformers listed in the Digest have aluminum or copper windings?

Product Line:
Dry Type Transformers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The NEMA 4X transformers, which are encapsulated, are only offered with copper windings. This is true for all encapsulated transformers offered by Square D.


CTA-ID : 2012732

Schneider Electric USA