{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
When upgrading a Powerpact P or R frame breaker from a Micrologic 3.0 to the 5.0P, 6.0P, 5.0H, or 6.0H trip units, what is needed to obtain voltage sensing?
Issue:
Upgrading powerpact P and R frame breaker Micrologic 3.0 to 5.0, 6.0P,5.0H or 6.0H Trip units.

Product Line:
Safety Switch

Resolution:
When upgrading to the P or H trip unit, an external voltage sensing kit must be installed.
Part numbers for field installable external voltage sensing kits are as follows:
S64203 for P frame unit mount/I-LINE
S64208 for R frame unit mount/I-LINE
S64209 for P frame drawout
S64210 for P frame motor operated/rotary handle

Schneider Electric USA