Issue:
What is the positive and neutral for the Tesys DC coils on contactors?
Product Line:
Contactors and Starters, IEC
Environment:
Tesys D Contactors
Cause:
Confirming which coil terminal is the positive, A1 or A2 on D Line Contactors.
Resolution:
As marked on the contactor, A1 is the positive terminal. Because of the built-in suppressor, they are polarity sensitive.
What is the positive and neutral for the Tesys DC coils on contactors?
Product Line:
Contactors and Starters, IEC
Environment:
Tesys D Contactors
Cause:
Confirming which coil terminal is the positive, A1 or A2 on D Line Contactors.
Resolution:
As marked on the contactor, A1 is the positive terminal. Because of the built-in suppressor, they are polarity sensitive.
Released for:Schneider Electric USA