{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is dashpot oil 9055R10P clear or colored red?
Issue:
What is the color of the 9055R10P dashpot oil?

Product Line:
Divested Products - Crane Control

Environment:
Product features

Resolution:
All dashpot oil is clear.

Note: Dashpot oil is part of Crane controls division that was divested to EC & M Crane Control. Contact them @ 1.336.434.2800 Ext. 2

Schneider Electric USA