Issue:
The list of repair parts is needed for Safety Switch catalog number H364AWK, series F6.
Product Line:
Heavy Duty Safety Switch
Resolution:
The repair parts for the H364AWK, series F6 (F06) are as follows. No other parts are available.
The list of repair parts is needed for Safety Switch catalog number H364AWK, series F6.
Product Line:
Heavy Duty Safety Switch
Resolution:
The repair parts for the H364AWK, series F6 (F06) are as follows. No other parts are available.
- Line Base Assembly - 4056703450 (1 required; includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
- Line Base mounting screws - 4020546401 (2 required per line base)
- Load Base Assembly - 4056677450 (1 required per phase; includes phynolic base, lugs, and fuse clips)
- Load Base mounting screws - 4020546401 (2 required per load base)
- Arc Suppressor Assembly - 4056677550 (1 required per phase)
- Arc Suppressor mounting screw - 4020514501
- Lug Assembly - 4025116251 (per lug)
- Lug Assembly mounting screw - 2140122240 (per lug)
- Switch Mechanism - 4056678650 (also requires switch mechanism gasket 4056786001)
- Switch Mechanism mounting screws - 2299940562 (2 required)
- Handle Assembly - 4056663550 (also requires handle gasket 4056603101)
- Lockplate - 4056672101
- Lockplate mounting screws - 2299940562 (2 required)
- Equipment Ground Lug Kit - PKOGTA2