{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the H363A, series F6? (may be shown as F06)
Issue:
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The replacement parts for the H363A, series F6 (F06) are as follows. No other parts are available.
Line Base Assembly - 4056775150 (1 required; arc suppressor assembly and fuse puller not included)
Load Base Assembly - 4056602850 (1 required)
Arc Suppressor Assembly - HAS0610F (includes arc suppressor, mounting screw, and instructions)
Fuse Puller Kit - FPK0610
Lug Assembly - 4025101851 (per lug)
Switch Mechanism - 4056646950 (also recommend replacing switch mechanism gasket)
Switch Mechanism Gasket - 4056603201
Handle Assembly - 4056663550
Handle Gasket - 4056603101
Lockplate - 4056672101
Line & Load base mounting screw - 4020515101 (3 for line and 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)
Equipment Ground Lug Kit - GTK0610

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: