Search FAQs
Is a pedestal type Meter Pak metering device available?
Issue:
Product Design
Product Line:
Meter Pak Metering
Resolution:
No pedestal type Meter Pak device is available. However, there are some Meter Pak wall mount wireway and wireway extensions that can give the appearance of a pedestal device.
NOTE: The wireway and wireway extensions CANNOT and DO NOT support any of the weight of a Meter Pak device. They are ONLY a wireway that attaches to the bottom side of a MP device for passing through the incoming supply conductors up to the device itself.
Product Design
Product Line:
Meter Pak Metering
Resolution:
No pedestal type Meter Pak device is available. However, there are some Meter Pak wall mount wireway and wireway extensions that can give the appearance of a pedestal device.
NOTE: The wireway and wireway extensions CANNOT and DO NOT support any of the weight of a Meter Pak device. They are ONLY a wireway that attaches to the bottom side of a MP device for passing through the incoming supply conductors up to the device itself.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: