{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the HU363DS, series F6? (may be shown as F06)
Issue:
Currrent design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The repair parts for the HU363DS, series F6 (F06) are as follows. No other parts are available.
Line Base Assembly - 4056775250 (arc suppressor not included)
-Line Base mounting screw - 4020515101 (3 required)
-Arc Suppressor Assembly - 4056635550 (Obsolete and replaced with part number NNZ51874)
-Arc Suppressor mounting screw - 4020514501 (1 required)
-Lug assembly - 4025101851 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: