Issue:
Checking on the replacement starter in an enclosed 2-pole NEMA size M-0 manual motor starter for AC applications.
Product Line:
2510 Type M Manual Starter
Environment:
Manual Starters and Switches
Resolution:
To replace only the starter, use the 2510MBO1 for the ones with the square push button operators or 2510TBO1 for the ones with the toggle operator.
Checking on the replacement starter in an enclosed 2-pole NEMA size M-0 manual motor starter for AC applications.
Product Line:
2510 Type M Manual Starter
Environment:
Manual Starters and Switches
Resolution:
To replace only the starter, use the 2510MBO1 for the ones with the square push button operators or 2510TBO1 for the ones with the toggle operator.