{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the life expectancy of the 9007C limit switches?
Issue:
Checking on the life expectancy of a 9007C limit switch.

Product Line:
9007 Limit Switches

Environment:
NEMA Limit Switches

Resolution:
Switches are tested to meet NEMA rating, but not tested to point of failure. Life depends on electrical load and number of mechanical operations together, and is not published

Schneider Electric USA