{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the H222DS, series F6? (may be shown as F06)
Issue:
Repair parts

Product Line:
HD SS

Resolution:
The repair parts for the H222DS, series F6 (F06) are as follows. No other parts are available.
-Line Base Assembly - 4056642150 (arc suppressor not included)
-Load Base Assembly - 4056002650
-Line & Load Base mounting screw - 4020516001 (3 for line and 2 for load)
-Arc Suppressor Assembly - HAS0610F
-Lug Assembly - 4025101652 (per lug)
-Lug Keps Nut - 2342501701 (per lug)
-Mechanism Assembly - 4056610750
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056699450 (also recommend replacing lockplate gaskets)
-Lockplate - 4056693201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101652 (2 required)
-Ground Lug Mounting Screw - 4020513503
-Fuse Pullers - FPK03 (1 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: