{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are replacement parts and auxiliary accessories still available for the Class 8502 and Class 8702 pre-type S contactors?
Issue:
Are replacement parts and auxiliary accessories still available for the Class 8502 and Class 8702 pre-type S contactors?

Product Line:
NEMA Contactors and Starters

Environment:
Obsolete Products

Cause:
Product selection

Resolution:
Some 31012-400-** (Type A Series B size 00 only) and 1861-S1-****(Type B All Series size 0) control coils may and still be available as they are also used with some active timing relay devices.
** & **** represent ending digets depending upon voltage required.

All other component parts, parts kits, coils, accessories, etc. are obsolete and no longer available.

If complete replacement device is required or desired, please use the Competitive Cross Reference tool link below.


CTA-ID : 2016563

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.