{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for a DIN rail Mounting Bracket for Class 8910 Definite Purpose Contactors?
Issue:
What is the form to use for a DIN rail Mounting Bracket for Class 8910 Definite Purpose Contactors?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Definite purpose Contactors

Resolution:
For All Class 8910 Type DP compact contactors, this is a factory modification. Order the contactor with form Y135.
For Class 8910 Type DPA (20 through 60 amp only) contactors order 9999DMB1. Not available for devices above 60 amp.

For Factory installed DIN Rail Bracket on 8910 DPA 20 through 60 amp contactors, order using Form Y135. For example, to order an 8910DPA12 with 120 volt control and DIN Rail attachment, part number will be 8910DP12V02Y135.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.