{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the wire range for the terminals provided on the PK32DGTA equipment ground bar?
Issue:
Product Features

Product Line:
Panelboard Accessory

Environment:
Products sold in North America

Resolution:
The PK32DGTA will accept (7) #6 AWG - 350 KCMIL Cu or Al wires and (18) #14 AWG - # 4 AWG Cu or Al wires.
This information is listed in Bulletin No. 2110PD9501.

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: