Issue:
Product Feature
Product Line:
INMVE - MV EQUIPMENT
Environment:
NEMA ICS 3, UL347, EEMAC G14-1, ANSI C19.7, IEC 60470, IEC 60529, IEC60694, IEC60129, IEC62271-102, IEC 62271-200, ANSI C37.20.7
Cause:
A NEMA 12 rating may be required for dirty, industrial environments.
Resolution:
No, Motorpact is only available in a NEMA 1 and NEMA 1A enclosure ratings.
Product Feature
Product Line:
INMVE - MV EQUIPMENT
Environment:
NEMA ICS 3, UL347, EEMAC G14-1, ANSI C19.7, IEC 60470, IEC 60529, IEC60694, IEC60129, IEC62271-102, IEC 62271-200, ANSI C37.20.7
Cause:
A NEMA 12 rating may be required for dirty, industrial environments.
Resolution:
No, Motorpact is only available in a NEMA 1 and NEMA 1A enclosure ratings.