{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the withstand rating for 8903 L & LX Lighting Contactors ?
Issue:
8903 L & LX Lighting Contactors withstand ratings.

Product Line:
NEMA Contactor and Starters

Environment:
Class 8903 Type L/LX Lighting Contactors

Resolution:
The contactor by itself has a 5K withstand rating.

This lighting contactor is suitable for use on a circuit capable of delivering not more than the rms symmetrical current at the maximum voltage shown below when protected by a 25 A UL Listed thermal-magnetic (inverse time) branch circuit breaker having interrupting ratings not less than shown below:
22,000 @ 240V
14,000 @ 480V
And, when protected by a 30 A UL Listed Class RK5 branch circuit current limiting fuse having interrupting rating not less than shown below:
100,000 @ 600V.

Schneider Electric USA