{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: The filler plate QOFP does not fit in some older QO load centers, is there another filler plate that works for the older QO load centers and how are they both installed?
Issue:
Load center accessory

Product Line:
QO load centers

Resolution:
There are two filler plates available for QO load centers, one for the older design and one for the current design QO load centers.
1) The part number QO1FP is a metal filler plate, for the OLDER load centers with twistouts measuring approximately 0.75" x 2.44"
2) The part number QOFP is a plastic filler plate, for the CURRENT load centers with twistouts measuring approximately 0.75" x 2.31". This filler plate may also fit some of the older style QO load centers that have the same twistout measurements.

The QOFP and QO1FP Filler plates are ONLY to be used for QO load centers to fill a branch breaker opening in the deadfront trim when a twistout has been removed and no branch breaker will be installed.

The filler plate, QO1FP is used with the older load centers that had the twistout sizes as mentioned above in #1 and should be installed as shown in the instructions that come with the kit.
The filler plate, QOFP is used with the current load centers that have the twistout size as mentioned above in #2 and should be installed as shown in the instructions that come with the kit.
The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger image

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the installation of the Branch Breaker opening filler plate by following the instructions.
2) Install the filler plate (A) from the front of cover (B) by pressing into place as shown
NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.



Label

Schneider Electric USA

Attachment(s)
QO1FP instructions.pdf [107.8 KB]
QOFP Instructions.pdf [80.31 KB]