{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the deadfront part numbers for an NF418M1 or NF418M1C interior?
Issue:
Deadfront for an NF418M1 or NF418M1C interior.

Product Line:
LV Panelboards

Environment:
NF Panelboards

Resolution:
Each panel will require the following:

(1) 80113-170-52 Back-fed Main Breaker Deadfront
(1) 80113-160-51 Branch Section
(1) 80113-174-50 Load End Cover

NOTE: These part numbers are now obsolete. Consider a local sheet metal fabricator, or replace the panel.

Schneider Electric USA