{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are 8536 & 8502 NEMA starters & contactors available with normally closed power contacts?
Issue:
Identify if there are normally closed power contacts available in the 8502 NEMA Contactors

Product Line:
8502 Contactors and 8536 Starters

Environment:
NEMA Contactors and Starters

Resolution:
These products are available ONLY with normally open power poles. Additional power poles to construct a 4- and 5-pole device are available with normally closed poles but this gives you a maximum of 2 normally closed poles and this is only available up through the NEMA size 2 starter or contactor.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.