{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the HU362AWK, series F6? (may be shown as F06)
Issue;
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The replacement parts for the HU362AWK, series F6 (F06) are as follows. No other parts are available.
-Line Base Assembly - 4056609150 (requires one per switch; arc suppressor assembly not included)
-Arc Suppressor Assembly - HAS0610F (includes arc suppressor and mounting screw)
-Lug Assembly - 4025101652 (per lug)
-Switch Mechanism - 4056646950 (recommend replacing switch mechanism gasket)
-Switch Mechanism Gasket - 4056603201
-Handle Assembly - 4056663550
-Handle Gasket - 4056603101
-Lockplate - 4056672101
-Line base mounting screw - 4020515101 (3 required)
-Arc Suppressor mounting screw - 4020514501 (1 required)
-Lockplate mounting screw - 2299940562 (2 required)
-Equipment Ground Lug Kit - GTK0610

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: