{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are replacement control circuit contact(s) available for the 9065 Melting Alloy Overload Relays?
Issue:
9065 Melting Alloy Overload Relays replacement aux contact

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA style Overload Relays

Resolution:
Yes, by NEMA contactor size as listed below:
Size 00 to 4, Size 5 (Series B) & Size 6 - standard normally closed control circuit contact, 9998SO1 or 9999SO4 standard normally closed control & (1) normally open isolated alarm contact or 9999SO5 standard normally closed control & (1) normally closed isolated alarm contact. For Size 5 (Series A) 31102-514-50 standard normally closed control circuit contact or 31102-514-51 for standard normally closed control circuit & (1) normally open (three point) alarm contact.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.