{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a three position, spring return to center selector switch for use with an XACA pendant station?
Issue:
22 mm selector switch spring return for XACA Pendant Station

Product Line:
Push Buttons

Environment:
22 mm operators

Resolution:
Yes, use. ZA2BD5. or any of the ZA2BD* or ZA2BG* operators

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: