{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the HU462AWK, series F6? (may be shown as F06)
Issue:
Repair Part

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the HU462AWK, series F6 (F06) are as follows. No other parts are available.
Line Base - one each of 4056625450 (left side base), 4056623050 (right side base), and 4056702801 (plastic connecting cam) (NOTE: arc suppressor not included).
Line Base mounting screws - 4020515101 (6 total required, 3 for each line base).
Arc Suppressor Assembly - HAS0610F (two required; includes arc suppressor and mounting screw)
Lug Assembly - 4025101652 (per lug)
Lug Mounting Screw - 4020514202 (per lug)
Mechanism Assembly - 4056646950 (also requires switch mechanism gasket 4056603201)
Handle - 4056663550 (requires handle gasket 4056603101)
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (requires 2)
Ground Lug - 4025101652 (2 total required)
Ground Lug mounting screw - 4020514801 (1 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: