{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are replacement contacts available for the Class 2510 / 2511 / 2512 Type M & T manual starters?
Issue:
What is the part number for the contact kit for 2510 / 2511 / 2512 Type M & T Manual starters?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 2510/2511 Type M/T Manual Starters

Resolution:
Yes, in three pole kits only. Select based on size of controller from below:
For Types MB & TB = 9998ML1
For Types MC & TC = 9998ML2

Note:
Class 2511 & Class 2512 devices include two manual starters and therefore two kits will be required.

Schneider Electric USA