Search FAQs
What is the maximum voltage rating that can be applied for the combination service entrance devices (CSEDs)?
Issue:
Product design specifications
Product Line:
Combination Service Entrance Devices
Resolution:
ALL CSEDs are single phase, 3 wire, 120/240 Vac maximum rated. So the maximum voltage is 240 Vac, single phase.
Product design specifications
Product Line:
Combination Service Entrance Devices
Resolution:
ALL CSEDs are single phase, 3 wire, 120/240 Vac maximum rated. So the maximum voltage is 240 Vac, single phase.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: