{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a GFI breaker be tested by creating a leakage to ground?
Issue:
Can we force a ground fault in order to ensure a GFI is working correctly?

Product Line:
Miniature Circuit Breakers

Resolution:
Yes, but this is not recommended. If the GFI is properly installed and functioning, the integral test button will trip the breaker. The test button creates a real ground fault through an 18000 ohm resistor. This is the only UL approved testing method.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.