{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the H361AWC, series F7 (may be shown as F07)?
Issue:
Design repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H361AWC, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056603950 (1 required; arc suppressor not included)
-Load Base Assembly - 4056604150 (1 required)
-Line and Load Base Mounting Screws - 4020515101 (3 for line, 2 for load)
-Arc Suppressor Assembly - 4056635550 (1 required)
-Arc Suppressor Mounting Screw - 4020514501 (1 required)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056787350 (NOTE: also recommend replacing switch mechanism gasket and handle gasket)
-Switch Mechanism Gasket - 4056786001
-Mechanism Washer - 2360200008
-Handle Assembly - 4056663550 (also recommend replacing handle gasket)
-Handle Gasket - 4056603101
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - 2541002806
-Receptacle Mounting Screws - 4510280101 (4 required)
-Ground Lug - 4025101652 (3 required)
-Ground Lug Mounting Screw - 4020513503 (2 required)
-Fuse Pullers - FPK03 (1 required)

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: