{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does Square D offer a meter socket 'jumper' cover that allows power (current) to pass through a meter socket without a Watt-hour meter installed?
Issue:
Meter Socket 'Jumper' Cover for the Metering Equipments

Product Line:
Metering Equipment

Environment:
EZM Metering and MP Meter-Pak Metering

Cause:
application

Resolution:
No.  Square D does NOT manufacture or offer a meter socket jumper cover.  A company called Ekstrom Industries, Inc. at 800-532-4332 or 248-477-0250 does manufacture Meter Socket Jumper Covers.  The jumper covers are a Lexan material with busbars attached to the back side and allows power (current) to pass through the meter socket without a Watt-hour meter installed.
NOTE: Square D does NOT ULtest or List third party components for use in its Metering product, so the customer assumes total responsibility for use of third party components.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.