Issue:
Selection
Product Line:
Enclosed GFCI Breaker
Resolution:
Two different products are available for this application: QOE250GFINM or HOME250SPA . The QOE250GFINM consists of a QO24L60NRNM (non-metallic) rainproof enclosure and a QO250GFI ground fault circuit interrupter. The QO24L60NRNM is also sold separately for other applications. The HOME250SPA consists of an HOM24L50R (metallic) rainproof enclosure and a HOM250GFI ground fault circuit breaker. The HOM24L50R is not sold separately.
Selection
Product Line:
Enclosed GFCI Breaker
Resolution:
Two different products are available for this application: QOE250GFINM or HOME250SPA . The QOE250GFINM consists of a QO24L60NRNM (non-metallic) rainproof enclosure and a QO250GFI ground fault circuit interrupter. The QO24L60NRNM is also sold separately for other applications. The HOME250SPA consists of an HOM24L50R (metallic) rainproof enclosure and a HOM250GFI ground fault circuit breaker. The HOM24L50R is not sold separately.