Search FAQs
What is the lug size in the Powerpact Q frame circuit breakers?
Issue:
What is the lug data for PowerPact Q frame breakers such as QB, QD, QG, QJ?
Product Line:
PowerPact Q frame Breakers
Resolution:
Powerpact Q frame circuit breakers have box type lugs suitable for a #4 AWG-300 kcmil single conductor, aluminum or copper. They are not removable or replaceable. Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: