{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the HU362DSWC, series F7 (may be shown as F07)?
Issue:
Repair parts list for HU362DSWC, series F7

Product Line:
Safety Switches

Resolution:
The repair parts for the HU362DSWC, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056609150 (1 required; arc suppressor not included)
-Line and Load Base Mounting Screws - 4020515101 (3 required)
-Arc Suppressor Assembly - 4056635550 (1 required)
-Arc Suppressor Mounting Screw - 4020514501 (1 required)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4053922550
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate Mounting Screw 2194918121 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - 2541000046
-Receptacle Mounting Screws - 4510280101
-Ground Lug - 4025101652 (3 required)
-Ground Lug Mounting Screw - 4020513503 (2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: