{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a QO-GFI or HOM-GFI breaker be used as a subfeed breaker to feed a downstream panel and provide the GFI protection to the entire subfed panel?
Issue:
Can a QO or HOM GFI breaker be used to feed a sub panel downstream

Product Line:
Miniature Circuit Breakers

Resolution:
Yes, BUT nuisance tripping may occur due to leakage from ALL the load conductors between the GFI breaker and subpanel and the bussing in the subpanel.

Schneider Electric USA