undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does Schneider Electric / Square D offer NEMA Type 7 or 9 Safety Switches for use in hazardous environments?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Cause:
Selection

Resolution:
HDSS = Heavy Duty Safety Switches
GDSS = General Duty Safety Switches
DTSS = Double Throw Safety Switches
SCCR = Short Circuit Current Rating

Square D does NOT offer any NEMA 7 or 9 switches for the GDSS or DTSS.


Square D does offer a few HDSS Types rated for NEMA 7 or 9, hazardous locations. See the current ON-LINE Digest for the catalog numbers.
DIGEST LINK

The NEMA 7 and 9 HDSS use Automatic Molded Case Switches and are considered NON-FUSIBLE and are NOT a Visible Blade Type design.
They are available in a 60Amp,100Amp and 225amp MAX. devices.
These devices are cULus Listed, except for 2 catalog numbers, the H225XJG and H225XJGAA, they are NOT cULus due to limited wire bending space.
These devices DO NOT have any SCCR, because there is NO internal overcurrent protection. When SCCR is required there MUST be upstream protection for the device.

FOR APPLICATIONS WHERE OVERCURRENT PROTECTION IS REQUIRED USE THE NEMA 7 and 9 MOLDED CASE CIRCUIT BREAKER ENCLOSURES. SEE CURRENT ON-LINE DIGEST SECTION 7

Schneider Electric USA

Does Schneider Electric / Square D offer NEMA Type 7 or 9 Safety Switches for use in hazardous environments?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches 

Cause:
Selection

Resolution:
HDSS = Heavy Duty Safety Switches
GDSS = General Duty Safety Switches
DTSS = Double Throw Safety Switches
SCCR = Short Circuit Current Rating

Square D does NOT offer any NEMA 7 or 9 switches for the GDSS or DTSS.


Square D does offer a few HDSS Types rated for NEMA 7 or 9, hazardous locations. See the current ON-LINE Digest for the catalog numbers. 
DIGEST LINK 

The NEMA 7 and 9 HDSS use Automatic Molded Case Switches and are considered NON-FUSIBLE and are NOT a Visible Blade Type design.
They are available in a 60Amp,100Amp and 225amp MAX. devices.
These devices are cULus Listed, except for 2 catalog numbers, the H225XJG and H225XJGAA, they are NOT cULus due to limited wire bending space.
These devices DO NOT have any SCCR, because there is NO internal overcurrent protection. When SCCR is required there MUST be upstream protection for the device. 

FOR APPLICATIONS WHERE OVERCURRENT PROTECTION IS REQUIRED USE THE NEMA 7 and 9 MOLDED CASE CIRCUIT BREAKER ENCLOSURES. SEE CURRENT ON-LINE DIGEST SECTION 7

Schneider Electric USA

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top