{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a mechanical interlock kit like the QO2DTI for use with (2) 3 pole QO breakers?
Issue:
Selection

Product Line:
QO Load Center

Resolution:
No, there is not. The QO2DTI can only be used to interlock between (2) 2-pole QO circuit breakers or (1) 2-pole and (1) 1-pole QO circuit breakers and there is no other mechanical interlock kit available.

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: