undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the terminal wire size and torque required for the STANDARD branch neutral bars in all Homeline and QO load centers?
Issue:
What is the terminal wire size and torque required for the STANDARD branch neutral bars in all load centers?

Product Line:
QO and Homeline Load Centers

Resolution:
The standard terminal sizes for the branch neutral bars in all the Homeline and QO load centers are shown below.

1) Homeline load center branch neutral bar terminal:
Wire Range TORQUE LB-IN
#4 CU/AL35
#6 CU/AL35
#8 CU/AL25
#10 - #14 CU20
#10 - #12 AL20

2) QO load center branch neutral bar terminals:
TORQUE LB-IN
Wire Range (AWG)Bar With 2 Screw Sizes
Large            Small
Bar With 1
Screw Size
1/0 - 3 CU/AL50              ... ...
4 CU/AL 45               ... 35
6 CU/AL45                 2535
8 CU/AL40                 1025
10 - 14 CU, 10 - 12 AL 35                10 20

Schneider Electric USA

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: