Search FAQs
Is there a version of Multi 9 breaker that has the terminal screws accessible from the rear?
Issue:
Can Multi 9 breaker connections be modified to allow access from the front or the rear?
Product line:
Modular circuit protection devices
Resolution:
The UL489 listed C60 breakers can be ordered with factory installed ring terminals, which allow for access from the rear. These are the C60BPR style Multi 9 devices. However, the standard box lug UL489 C60BP breakers do not allow access to the terminals from the rear and cannot be converted in the field with the 17400 ring tongue terminal kit. The UL489 C60BP breakers are only accessible from the front.
The 17400 ring tongue terminal kit allows access from the rear and will convert the connection type from a standard box lug to a ring tongue terminal. It accepts UL Listed or CSA Certified insulated ring terminal only, max width: 0.54 in or 13.9 mm. Only for use on:
Can Multi 9 breaker connections be modified to allow access from the front or the rear?
Product line:
Modular circuit protection devices
Resolution:
The UL489 listed C60 breakers can be ordered with factory installed ring terminals, which allow for access from the rear. These are the C60BPR style Multi 9 devices. However, the standard box lug UL489 C60BP breakers do not allow access to the terminals from the rear and cannot be converted in the field with the 17400 ring tongue terminal kit. The UL489 C60BP breakers are only accessible from the front.
The 17400 ring tongue terminal kit allows access from the rear and will convert the connection type from a standard box lug to a ring tongue terminal. It accepts UL Listed or CSA Certified insulated ring terminal only, max width: 0.54 in or 13.9 mm. Only for use on:
- UL1077 Recognized C60 Supplementary Protectors
- UL1077 Recognized C60H-DC Circuit Breakers
- IEC Certified C60N/H/L and C60CTRL Circuit Breakers
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: