{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How many thermal units are used with a 2510 Type M 3 phase unit?
Issue:
Need to know the number of thermal units he needs for the 2510M/T manual starters.

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 2510 Starters

Resolution:
Three thermal units are required for 3 phase operation

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.